Every Overhaul. Lasting Value.
To the naked eye, most overhaul kits look pretty similar. The pistons have the same shape and the same number of rings, gaskets
appear to be made of the same material, the only obvious difference is the price. So what makes a Genuine Cummins TriTech
Overhaul Kit worth more than the "will-fit" competition? Extensive testing and stress analysis show significant differences
in design and manufacturing. Close examination proves that Cummins TriTech Overhaul Kit parts will last longer and perform
better - making them the best value for your next overhaul.
Every Piston. Stronger.
Ever see a cracked piston? It usually starts around the pin bore, where the constant up-and-down motion adds stress to the
area around the hole. Cummins pistons are made with a higher silicon content and less porosity than competitive pistons, so
they have up to 17% greater resistance to the forces that cause piston cracking and premature failure.
Every Ring. Machined.
Under the microscope, it's easy to see the difference between Cummins TriTech rings and those of the competition. The outer
surface of our top ring is machined for superior control of blowby gases. Our second ring is chrome-coated for longer life.
Our oil control ring has a variable pitch spring that adjusts for wear, while other manufacturers cut corners and use a constant
pitch spring, which can lead to excess oil consumption.
Every Liner. Crosshatched.
Using a microscope, you can see a very fine crosshatch pattern ground into the inside surface of every Cummins TriTech cylinder
liner. These lines form a diamond pattern where the oil gathers and stays, providing a more even layer of protection between
the piston rings and the liner. Competitive liners don't have any kind of cross-hatching. This extra step in the machining
of Cummins TriTech cylinder liners improves lubrication and reduces wear on the rings.
Every Bearing. Cast.
Without getting deeply into the world of metallurgy, there are two different ways to make a bearing. You can cast them in
a single piece using molten metal and a form, or you can use powdered metal as our competitors do, and "sinter" them into
the desired shape. Obviously, when you're talking about a part that bears the full load of the engine as it is transferred
to the crankshaft, stronger is better. Cummins TriTech bearings are cast, which gives them improved wear resistance and as
much as 15% more fatigue strength when compared to sintered bearings. What happens when a sintered bearing breaks apart? Very
often, you have to replace the entire block, which can cost thousands of dollars.
Every Head Gasket. Tougher.
There's even a difference in head gaskets, although you might not know it until your engine reaches about 200C. That's where
competitive gaskets start to fail, which can lead to coolant leaks outside - or inside - your engine. The grommets in the
head gaskets in Cummins TriTech Overhaul Kits are designed to withstand temperatures of at least 240C to prevent coolant leaks,
unlike the silicone grommets of the competition. Additionally, Genuine Cummins cylinder head gaskets are made of aluminized
steel, which is more durable than painted or moly-coated "will-fit" gaskets. Finally, Genuine Cummins head gaskets include
a rubber edge molding around the outside of the gasket, providing an added layer of protection against outside elements such
as road salt which can cause corrosion of the cylinder head and block mating surfaces.
Every Oil Pan Gasket. Thicker. Stronger.
There are both visible and invisible differences in the oil pan gaskets that directly correlate to performance. The Genuine
Cummins oil pan gasket is made of MP15 material, providing superior bolt torque retention and low clamping force sealing compared
to "will-fit" gaskets made of TS9016 or TS9003. Further, the Cummins oil pan gasket is 60% thicker than the non-genuine gaskets,
providing additional protection.
Every Start-Up. Smooth.
Cummins TriTech Overhaul Kits include a finer phosphate coating on the liners, which helps improve the seating of the rings
and reduces the potential for damage upon initial start-up. Competitive overhaul kits use a coarser grade of phosphate, which
is similar to using a heavy grit of sandpaper.
Every TriTech Overhaul Kit. Guaranteed.
Of course, the biggest difference is the company that stands behind its product. Every Cummins TriTech Overhaul Kit is fully
warranted for materials and workmanship for up to 3 years/300,000 miles (482,804 km) on our Cummins TriTech Plus dual Ni-Resist
pistons. So you can look forward to many more years of dependable, durable service from your Cummins engine with complete
confidence.
Every Question. Answered.
To learn more about Cummins TriTech Overhaul Kits, phone 1-800-CUMMINS(1-800-286-6467) or visit your local Cummins dealer
or distributor.
Bulletin: 4081641
Updated: 07/11/06