System Requirements   

System requirements for optimal use of QuickServe Online are as follows:

  • Personal Computer
    • Apple Mac OS X (10.4+)
    • Linux (Ubuntu/RedHat/OpenSuse/etc.)
    • Solaris 10/OpenSolaris
    • Windows (2000/XP/Vista/7)
    • Monitor capable of a minimum screen resolution of 1024x768.
  • Internet Connection
    • Broadband (Cable/DSL/T1) (Recommended)
    • 56K Dial-Up Modem (Minimum)
  • Web Browser (JavaScript and acceptance of Cookies must be enabled.)
  • Some content on QuickServe Online requires the use of software to display PDF files, such as Adobe Acrobat.
  • Some content on QuickServe Online requires the use of the Adobe Flash player plugin.

 

For optimal browser performance while using Internet Explorer, please follow the steps below:

In Internet Explorer, select Tools >> Internet Options >> General >> Browsing History >> Settings. A new window should open, and you should see "Check for newer versions of stored pages:" Be sure that "Every time I visit the webpage" is selected and then click OK.

IAC
J1939 Data Link Diagnostic Tool
NOx Sensor Test
Diesel Exhaust Fluid (DEF) Voltage Drop Test
Volvoline